HCS08DZ60 PIN bit in SRS Register is not set

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HCS08DZ60 PIN bit in SRS Register is not set

2,115 次查看
wander_zhang
Contributor I

Hallo all,

 

I have a Probem the SRS registers.

the Definiton of the SRS is

---------------------------------------------

bit7   bit6   bit5   bit4   bit3   bit2  bit1   bit0

POR   PIN   COP   ILOP  ILAD  LOC  LVD    --

---------------------------------------------

I generate a Reset signal on the Reset Pin of the µC and the µC will reset itself. After that I read the SRS Register somewhere in the code, I get a value of sometimes 0x40 (PIN ist set), and sometimes 0x2(LVD is set).  Wha I expect is that the bit6 "PIN" should always be set. I can't understand why the LVD bit is set and if it is set why the bit "PIN" is not set?

 

Thank you!

 

Zhang

标签 (1)
0 项奖励
回复
2 回复数

1,309 次查看
Nik
Contributor III

I have the same problem.  Did you solve this?

Thanks,

-

Robert

0 项奖励
回复

1,309 次查看
wander_zhang
Contributor I

It was a long time ago. But I dont think the problem is resolved.

 

regards

Chunyu

 

 

 

0 项奖励
回复