HC908GR16 -32  and HC908GZ16 -32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HC908GR16 -32  and HC908GZ16 -32

2,608 次查看
mbandini
Contributor I
What's the differents beetwin HC908GR16 -32  and HC908GZ16 -32
 
And why I can't find GZ16 32 all over the world?
标签 (1)
0 项奖励
回复
3 回复数

1,606 次查看
mbandini
Contributor I
So if I dont'use msCAN bus
 
But I use a external Oscillator with 16MHz TTL output
 
I can Use GR16 32 pin, they are pin to pin compatible isn't it?
 
I need to Recompile the firmware or not?
0 项奖励
回复

1,606 次查看
Alban
Senior Contributor II
Hello,

You don't say which one you use now. So can't tell you much.
External square wave of 16MHz will work on all mentioned.

Comparing the pinout, register map, and errata published is the best way for you to assess drop-in replacement.

Alban.
0 项奖励
回复

1,606 次查看
Alban
Senior Contributor II
Hello,
 
GR should not have a msCAN module and low frequency oscillator (32kHz XTAL typ.)
GRxxA should not have a msCAN module and high frequency oscillator (>1MHz XTAL)
GZ have a msCAN module and high frequency oscillator (>1MHz XTAL)
 
They are all available and shipped around the world. (except countries with an embargo, that goes without saying).
 
Alban.
0 项奖励
回复