For save power--about STOP mode and KBI-MC13213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For save power--about STOP mode and KBI-MC13213

2,201件の閲覧回数
Beijing2008
Contributor I
Hi all:
  I'm using CodeWarrior6.1 and MC13213(HCS08).
 
  I would like to get a answer from you.My problem as follows:
  "The KBI(keyboard interrupt) will be disable if HCS08 turn into the STOP1 or STOP2 mode,but in STOP3 mode, the KBI is enable",is it Right about above description??
  Currently,I add some codes as below for going into the STOP1 mode,add up to 7 lines:

#define ENTER_LOW_POWER _asm stop
#define MCU_STOP3_MODE()    SPMSC2 = 0x04; ENTER_LOW_POWER;        
#define MCU_STOP2_MODE()   SPMSC2 = 0x07;ENTER_LOW_POWER;                    
#define MCU_STOP1_MODE()    SPMSC2 = 0x06; ENTER_LOW_POWER; 
//.enter STOP1...
UseMcuClock();
(void)MLMEHibernateRequest();
MCU_STOP1_MODE();

But then,I press the button on PCB,it still can trigger the KBI and light one LED.Why??
My aim is save power.
Maybe any register hadn't been config successfully,please give me some hints.
 
Thanks and best regards,
Charly
ラベル(1)
0 件の賞賛
返信
1 返信

1,165件の閲覧回数
Beijing2008
Contributor I
Hi,all:
 
  Maybe the above description was not clear,I'm very sorry!
 
  In short,I want to know how to enter the STOP1/2/3 mode with HCS08(bind in the MC13213)? How to test the save power effect?  And how to wake up it from STOP mode?
 
Thanks and best regards,
Charly
 
 
0 件の賞賛
返信