Flextimer PWM sync between 2 Microcontrollers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flextimer PWM sync between 2 Microcontrollers

931 Views
abicash
Contributor III

Hello

 

Is there a way to use external trigger to synchronise a FTMxCHn and FTMxCHn+1 with another Microcontroller running the same frequency PWM?

 

The situation is like this

I have a Flextimer running 4 channels (each pair is complementary-combined) on MCU1

I have the same situation in MCU2.

I require the Flextimer in MCU1 to be run as slave to MCU2, being triggered by FTMxCHn out of MCU2 in MODE1

and self triggered (Software triggered in MODE2)

 

Can someone share an idea how this can be achieved?

Labels (1)
0 Kudos
Reply
0 Replies