Flashing EEPROM to S9S08EL32 MCU problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing EEPROM to S9S08EL32 MCU problem

1,981 Views
Alex_Glide
Contributor I

Hi all!

I work with old device, built on NXP/Freescale S9S08EL32 MCU and I have a problem with it. I need to program EEPROM on this MCU, but I can't. 

I using an USBDM Programmer and every time I trying to flash an EEPROM the USBDM Programmer send me an error "Access to PPAGE register failed".

How many pages of EEPROM MCU has and what I need to change in USBDM Programmer?

What I need to do to flash EEPROM correctly?

 

0 Kudos
Reply
8 Replies

1,912 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

Could you share which OS and IDE are you using please?

Could you help us confirm that you installed the drivers for USBDM?

The EEPROM has 2 pages (Page 0 and Page 1) the access in memory map is described in the MC9S08EL32: Data Sheet for MC9S08SL16 and MC9S08EL32 Series MCUs Chapter 4.5.11.3

Additionally in Chapter 4.5.2 indicate some configurations to do before any program or erase command can be accepted.

Best Regards

0 Kudos
Reply

1,801 Views
Alex_Glide
Contributor I

I'm using Windows 10 x64 Professional Edition. For programming my MCU I'm using USBDM Programmer (hardware) and USBDM Software ver. 4.12.1.340 and USBDM 4.12.1.325. The hardware programmer's firmware 4.12.2. USBDM Programmer is chinese replica, bought on Aliexpress. Drivers for USBDM installed. 

Alex_Glide_0-1775763097374.png

Alex_Glide_1-1775763118906.png

Alex_Glide_2-1775763134153.png

I've read about EEPROM memory in datasheet, but I don't know, what and where I need point out any configuration options of EEPROM programming.

0 Kudos
Reply

1,787 Views
luis_maravilla
NXP Employee
NXP Employee

The USBDMs in AliExpress are not an official NXP product, Sorry for the inconveniences this might have caused you.

I would recommend you contact the manufacturer or vendor on this for supporting the product.

 

Also, you could try using CodeWarrior® for MCUs (Eclipse IDE) v11.1 that support MC9S08EL32 using the compatible programmers to flash the device.

0 Kudos
Reply

1,936 Views
db16122
Contributor IV

64BYTES for EEPROM SIZE according to the RM for MC9S08 but you may refer to the AN5233 for program setup guideline. Is there any error code or error log?

0 Kudos
Reply

1,800 Views
Alex_Glide
Contributor I

Every time I trying to program my MCU the software return error message "Access to PPAGE register failed!"

I think it's because of my attempts to program EEPROM memory without any attributes or options enabled. And I don't know what to do. 

0 Kudos
Reply

1,468 Views
db16122
Contributor IV

BTW, why not try codewarrior IDE to program instead? Third party tools may be hard to support from MCU vendor side

0 Kudos
Reply

1,955 Views
db16122
Contributor IV

do you want to program eeprom emulated on MCU chip or you want to program on seperated EEPROM from SPI or I2C?

0 Kudos
Reply

1,947 Views
Alex_Glide
Contributor I

I want to program eeprom inside MCU. I haven't any memory chip on my board.

0 Kudos
Reply