Flash Programming for MC9RS08KA2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programming for MC9RS08KA2

1,961 Views
seiji
Contributor I
I want to use 2 bytes flash of MC9RS08KA2 for config, but I see that:

Flash memory cannot be programmed or erased by software code executed from flash and device does not include on-chip charge pump circuitry, external VPP is required for program and erase operations.

I would like to know if I put external Vpp and run the flash programming procedure from RAM. Can I program flash? If possible, someone have an example for this.

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,225 Views
Alban
Senior Contributor II
Hello & Welcome Seiji,
 
You don't only need Vpp outside but also a very special circuitry.
I don't have the details of the circuitry itself but you need to respect timings with Vpp.
 
Please look at the datasheet that surely explains better than I am now.
Cheers,
Alban.
0 Kudos
Reply