FXTH871 PWU Flag Bits Unresponsive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXTH871 PWU Flag Bits Unresponsive

944 Views
csaunders9526
Contributor I

Hello Community,

I am running in to a problem with the FXTH871, in particular with the PWU Flag Bits.

There are 2 flag bits that I can see that on the datasheet say will be set whenever a Periodic Wake Up is what removes the MCU from SLEEP modes.  These 2 bits are: PWUCS0_WUF & SIMSES_PWUF.

----------------------------------------------------------------------------------------------------------------------------------------

*From the datasheet:

PWUCS0_WUF: Wakeup Interrupt Flag — The WUF bit indicates when a wakeup interrupt has been generated by the PWU. This bit is cleared by writing a one to the WUFAK bit. Writing a zero to this bit has no effect. Reset clears this bit.

SIMSES_PWUF: PWU Flag — This bit indicates that the PWU module caused the last exit from STOP mode.

----------------------------------------------------------------------------------------------------------------------------------------

Neither of these bits seems to be set when I use PWU to wake up the MCU from SLEEP modes.  I am certain that the PWU is responsible for the wake up as well because I can adjust the time on the PWU, and it correctly wakes up at whatever time I set it to.

I have attached the very simple code that I am running right now to this post.  I am hoping that somebody can answer to me

Tags (3)
0 Kudos
Reply
0 Replies