ESD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ESD

3,690 Views
admin
Specialist II
Hello! I'm new in this forum. I would want find if the microcontrollers, in special if the mc68hc908gp32 can resist discharges ESD. It's resistant to these discharges?  What recommends to me so that it is not damaged because of this?
I will thank for this aid.
Good bye.
Labels (1)
0 Kudos
Reply
2 Replies

1,931 Views
glork
Contributor I
Hello AFVR.
This is a good question. I looked only at the MC9S08GB/GT manual, it includes a statement on ESD on page 259, section A4. I'll patch it in here:
"
Electrostatic Discharge (ESD) Protection Characteristics
A.4 Electrostatic Discharge (ESD) Protection Characteristics
Although damage from static discharge is much less common on these devices than on early CMOS
circuits, normal handling precautions should be used to avoid exposure to static discharge. Qualification
tests are performed to ensure that these devices can withstand exposure to reasonable levels of static
without suffering any permanent damage. All ESD testing is in conformity with CDF-AEC-Q00 Stress
Test Qualification for Automotive Grade Integrated Circuits. (http://www.aecouncil.com/) This devicewas
qualified to AEC-Q100 Rev E. A device is considered to have failed if, after exposure to ESD pulses, the
device no longer meets the device specification requirements.
"
As a personal statement I've been designing Freescale/Motorola microcontrollers into embedded products for more than 15 years and have never had a known ESD failure.
ron
0 Kudos
Reply

1,931 Views
admin
Specialist II
I always have trusted in products of Freescale, and now I know that will be difficult that they are damaged in my hands :smileytongue:, are very good, but is necessary be careful.  :smileyhappy:
Thanks for the answer!
0 Kudos
Reply