Does anyone have experience in MC9S08AW32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does anyone have experience in MC9S08AW32

1,425 次查看
Daniel_FE
Contributor I
Hi all:

I'm a newbie in HCS08.

Now, I have a problem about the TPM in MC9S08AW32.

I use the 4MHz crystal and set the bus clock to 20MHz.
And I want to set a interrupt per 500usec.
So I use the TPM module, but it isn't work to me.
I don't know what's happen?

Does anyone can help me,thanks.

My workaround:
Codewarrior V3.1 for HC(S)08

Below is my code.


#include // For enable interrupts macro
#include // Include peripheral declarations
#define LED1 PTCD_PTCD2

interrupt Vtpm1ovf void TPM1OVFISR(void)
{
if(TPM1SC_TOF) // 500us
{
TPM1SC_TOF=0;
LED^=1;
}
}

void IniCpu(void)
{
---------
---------
PTADD=0b00000000; // I/O data direction, 1:smileysurprised:utput, 0:Input
PTBDD=0b00000000; // I/O data direction, 1:smileysurprised:utput, 0:Input
PTCDD=0b01011100; // I/O data direction, 1:smileysurprised:utput, 0:Input
// Set the PTC5 is a SCI Rx2,PTC3 is SCI Tx2
PTDDD=0b00000000;
PTEDD=0b00000001; // Set the PTE1 is a SCI Rx1,PTE0 is SCI Tx1
PTFDD=0b11110000; // Set PTF[6:7] are output, PTF[4:5] are PWM output
PTGDD=0b00000000;
----------
----------

// --- Timer1 configuration ---
TPM1SC_PS = 0; // Select prescale = 1
TPM1MOD = 10000;
TPM1SC_CLKSB=0;
TPM1SC_CLKSA=1; // Select bus clock
TPM1SC_TOF=0;
TPM1SC_TOIE = 1;
}

void main(void)
{
SOPT=0x00; // Disable cop module
IniPLL(); // Initial PLL module
IniCpu(); // Initial Cpu

EnableInterrupts; // Enable interrupts
for(;:smileywink:
{
__RESET_WATCHDOG();


}
}
标签 (1)
0 项奖励
回复
1 回复

696 次查看
thisobj
Contributor III
Hello Daniel,

You haven't configured the TPM1C1SC register. Page 170 of MC9S08AWxx.pdf shows the bits in this register.

Frank
0 项奖励
回复