Debugger for OSEK turbo application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger for OSEK turbo application

2,200 Views
tupham
Contributor I
Dear all,
 
I have installed Code Warrior for HC(S)08 v5.1 and OSEK turbo v2.3. I have built sample for HC08GZ60 which is available after installing OSEK turbo. I have followed steps to build that sample application and generate all necessary files in 3 folders: bin, gen, obj. Especially in bin, I have the executable file "sample.hex" and the link file "sample.map". But till now, I don't know what the "debugger" is. Is it Code Warrior v5.1? I can't find how to use the debugger in Code Warrior v5.1 to execute that OSEK application. Please help me.
 
Thanks anyway,
 
Tu Pham.
Labels (1)
0 Kudos
Reply
1 Reply

1,127 Views
CrasyCat
Specialist III

Hello

What happens if you select Project -> Debug?

This should load code on the target and start the debugger.

CrasyCat

0 Kudos
Reply