DEMO9S08QG8_APP Error.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEMO9S08QG8_APP Error.

2,126件の閲覧回数
Dimy
Contributor I
Hello, a got the source for the DEMO9S08QG8_APP from the forum and I can't compile the file because of an error in codeWarrior: c4402 Redefinition of existing macro 'NVICSTRM'.
I didn't made any alteration to the source, so I am not sure what to do.
Any help would be appreciated.

Dimy.
ラベル(1)
0 件の賞賛
返信
1 返信

1,293件の閲覧回数
bigmac
Specialist III
Hello Dimy,
 
I have not checked, but it is possible that this macro may already be defined within the header file for the QG8 device.  If this is the case, you can probably "comment out" the second definition of the macro within the project file.
 
The demo code may have originally been compiled using an earlier version of CW that did not already contain the macro definition.
 
Regards,
Mac
 
0 件の賞賛
返信