Codewarrior 6.3 , USB P&E MULTILINK   ERROR 18 during script!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 6.3 , USB P&E MULTILINK   ERROR 18 during script!

1,883 Views
song
Contributor I

I'm using the Codewarrior 6.3 , the USB P&E MULTILINK and MC9S08GB60 processor

 

on downloading ...

  

CMD>PM

Programming and Verifying Address $0C000 Error during  programming.

ERROR 18 during script!

 

 

What can I do to solve this problem.

Labels (1)
0 Kudos
Reply
1 Reply

1,185 Views
jojoba
Contributor I

Hi

 

Quickest solution is you can replace the microchip. get 2-3 ordered from freescale.

I had issue with this for two days .... and struggled with it .

 

You can still program it using expert mode programmer though!

0 Kudos
Reply