Can't make LF interrupt work! FXTH8715 tried everything

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't make LF interrupt work! FXTH8715 tried everything

1,105 次查看
javierpernia
Contributor I

Hi everyone, i have been working with FreeScale FXTH87x for sending Pressure and Temperature at 434MHz. now i want to be able to activate de chip using Low Frequency at 125Khz. For now, i want the simples activation, i dont need to check data nor SYCN WORDS, only carrier. 

im been following the datasheet and the TPMS_FXTH87_LF_RF_Comunication example. and i took special attention to the function void vfnDataModeInit(void)  in szk_lf_data_detect.c changing it, with not luck of making it work.

Im using a MaxiTPMS TS401 as the activator.

0 项奖励
回复
0 回复数