Can't get interrupt vector to link into my application on MC9S08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't get interrupt vector to link into my application on MC9S08

Jump to solution
2,649 Views
Mr_Freez
Contributor II

Hello

I am having a problem getting my linker to not dead-strip my interrupt service routine out of my application code.  I have searched the forum for similar posts and many refer to either using FORCE_ACTIVE in my linker command file OR using #pragma force_active on around my isr.

I have tried all of these and nothing works.  I believe that the problem is syntax??

Does anyone have any suggestions?  You'd think this would be well documented somewhere??

 

Thanks

Rich

Labels (1)
0 Kudos
Reply
1 Solution
1,164 Views
Mr_Freez
Contributor II
Thanks! that app note solved numerous problems...

View solution in original post

0 Kudos
Reply
3 Replies
1,164 Views
CompilerGuru
NXP Employee
NXP Employee

For the S08 the prm file command to add reference roots is ENTRIES.

E.g. "ENTRIES main Table END "

 

FORCE_ACTIVE or the force_active pragma are supported for the ColdFire architecture, check for which architecture a particular forum entry is. The ENTRIES topic came up often for the S08 too in the past.

 

Daniel

0 Kudos
Reply
1,164 Views
bigmac
Specialist III

Hello Rich, and welcome to the forum.

 

There are a number of possibilities available for coding interrupts.  Application note AN2616 briefly describes some of them (within the FAQ section).

 

Perhaps you might alternatively use the PE device initialisation tool when you create the project.  This will provide a framework for your interrupts, including generating a vector table.

 

Regards,

Mac

 

0 Kudos
Reply
1,165 Views
Mr_Freez
Contributor II
Thanks! that app note solved numerous problems...
0 Kudos
Reply