Can I use chips from this source to accomplish my task or do they need to be purchased from PJRC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use chips from this source to accomplish my task or do they need to be purchased from PJRC?

1,171 Views
gigatech
Contributor I

Hi guys,

I am currently working on commercializing my first design and am using the teensy 3.5 to prototype.
I am wondering if I can use the MKL02Z32FG4 chips sold here:

http://uk.farnell.com/nxp/mkl02z32vfg4/mcu-32bit-cortex-m0-48mhz-qfn16/dp/2409470?ost=MKL02Z32VFG4&d...

in the same manner as they are used here:

PJRC Store 
IE, to bootload a MK64FX512VLL12 chip via teensyduino ( A teensy bootloader plugin mounted within arduino studio).
Any help or general advice on this matter would be greatly, greatly appreciated as I am something of a novice to creating boards of this complexity and am working alone.

Thanks in advance,

Giga.

0 Kudos
Reply
0 Replies