CAN filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN filter

Jump to solution
4,970 Views
francy
Contributor I

I use MC9S08DZ60 and I must make a CAN application, but I am not able to do the can filter.

I set the CANIDAC register fo two filter of 32 bit, the CANIDAR0/3 registers with my ID that I want to filter and the CANIDMR0/3 with the mask, how it is written on data sheets, but it does not function

 

I write the example that I am doing

CANIDAC=0x00  obviously written with its procedure

 

CANIDAR0=0x18

CANIDAR1=0xFF

CANIDAR2=0x00

CANIDAR3=0x00

 

CANIDMR0=0x00

CANIDMR0=0x00

CANIDMR0=0xff

CANIDMR3=0xff 

 With this mask I want to applicate the filter only at the four initial byte and the other are do not care.

 

Can someone help me? Does someone know what I make the mistake?

Thanks.

Bye

Labels (1)
0 Kudos
Reply
1 Solution
3,075 Views
kef
Specialist I

francy wrote:

CANIDAR0=0x18

CANIDAR1=0xFF

CANIDAR2=0x00

CANIDAR3=0x00

 

I do not understood:

"So IDs accepted are from (1<<25)|(1<<24)|(0x3F <<15) = 0x31F8000 to 0x31F807F, both RTR=1 and RTR=0"

 


Bit4 from CANIDAR0 is ID25 (bit25 of extended CAN identifier), that's 2^25 or 1<<25

Bit3 from CANIDAR0 is ID24, 1<<24

All CANIDAR1 bits are set, that's 6 conseutive bits from ID20 to ID15. Binary consisting of 6 ones equals 2^6 -1 = 0x3F. Least of these bits is bit15 of CAN identifier, so we need to shift 0x3F left by 15 bit positions, 0x3F << 15.

 

You want to accept 0x18FF0000 to 0x18FFFFFF. 0x18FF0000 identifier has ones from bit16(ID16) to bit28(ID28) (not as you said id20 to id13). Now look again at extended id mapping.

 

CANIDAR0 = 0xFF; // ID28..ID21 are set

CANIDAR1 = 0xE6 | 0x18; // ID20..ID16 are set, plus IDE and SRR are set

 

Since all other bits (and probably RTR, you didn't say) are don't care, you don't have to set up CANIDAR2 and CANIDAR3.

 

Now masks.

CANIDMR0 = 0; // received ID28..ID21 have to match what's specified in IDAR0

CANIDMR1 = 1; // received ID20..ID16 (but not ID15), IDE, SRR have to match what's specified in IDAR1

CANIDMR2 = 0xFF; // ID14..ID7 are don't care

CANIDMR3 = 0xFF; // ID6..ID0 and RTR are don't care

View solution in original post

0 Kudos
Reply
4 Replies
3,075 Views
kef
Specialist I

See attached pictures from datasheet. One picture shows Standard identifier (IDE=0) mapping (which ID bit in which Tx/Rx buffer register/register_bit). Another picture shows the same for Extended identifier (IDE=1, SRR=1).

Acceptance filters, both IDARx and IDMRx have exactly the same ID mappings.

IDMRx bit set to '1' makes corresponding IDRx bit don't care (bit is passed). IDMRx bit set to '0' makes filter passing only if corresponding IDRx bit matches corresponding IDARx bit.

If 8 bit mode, acceptance filters analyse only IDR0 register. In standard mode, thats ID bits ID10 to ID3. In extended - ID28 to ID21. All other ID bits are don't care.

In 16bit mode, IDR0 and IDR1 registers are analysed.

Is it now more clear?

 

Let's analyse what's your setup would accept. You didn't setup CANIDMR1 and CANIDMR2. As docs say, by default IDMRx are reset to 0. So CANIDMR0-CANIDMR2 = 0, CANIDMR=0xFF. IDR3 bits are don't care, IDR0-IDR2 bits have to match IDAR0-IDAR1 bits.

CANIDAR1 = 0xFF, so IDE=1 and SRR = 1, so only eExtended identifier messages are accepted.

CANIDAR0= 0x18, so ID25=1, ID24=1.

CANIDAR1=0xFF, so ID20..ID15=1

 

CANIDMR3 = 0xFF, so all combinations of ID6..ID0 are accepted.

 

So IDs accepted are from (1<<25)|(1<<24)|(0x3F <<15) = 0x31F8000 to 0x31F807F, both RTR=1 and RTR=0.

 

Try using search at bottom of this page. It should reveal some more answers.

0 Kudos
Reply
3,075 Views
francy
Contributor I

Hi kef,

 

I have alredy seen that picture on datasheet and I am using the extend identifier.

 

In my example I made a mistake of writing; the correct configuration is

CANIDAR0=0x18

CANIDAR1=0xFF

CANIDAR2=0x00

CANIDAR3=0x00

 

CANIDMR0=0x00

CANIDMR1=0x00

CANIDMR2=0xff

CANIDMR3=0xff 

 

I do not understood:

"So IDs accepted are from (1<<25)|(1<<24)|(0x3F <<15) = 0x31F8000 to 0x31F807F, both RTR=1 and RTR=0"

I want that IDs accepted are from 0x18ff0000 to 0x18ffffff. How can I do?

 

I also used another configuration

CANIDAR0=0x18

CANIDAR1=0xFF

CANIDAR2=0xC0

CANIDAR3=0x00

 

CANIDMR0=0x00

CANIDMR1=0x00

CANIDMR2=0x3f

CANIDMR3=0xff 

 so from id20 to id13 are 1 and srr and ide are also 1,but the result don not change.

I am not able that IDs accepted are from 0x18ff0000 to 0x18ffffff

 

 

Thanks

 

0 Kudos
Reply
3,076 Views
kef
Specialist I

francy wrote:

CANIDAR0=0x18

CANIDAR1=0xFF

CANIDAR2=0x00

CANIDAR3=0x00

 

I do not understood:

"So IDs accepted are from (1<<25)|(1<<24)|(0x3F <<15) = 0x31F8000 to 0x31F807F, both RTR=1 and RTR=0"

 


Bit4 from CANIDAR0 is ID25 (bit25 of extended CAN identifier), that's 2^25 or 1<<25

Bit3 from CANIDAR0 is ID24, 1<<24

All CANIDAR1 bits are set, that's 6 conseutive bits from ID20 to ID15. Binary consisting of 6 ones equals 2^6 -1 = 0x3F. Least of these bits is bit15 of CAN identifier, so we need to shift 0x3F left by 15 bit positions, 0x3F << 15.

 

You want to accept 0x18FF0000 to 0x18FFFFFF. 0x18FF0000 identifier has ones from bit16(ID16) to bit28(ID28) (not as you said id20 to id13). Now look again at extended id mapping.

 

CANIDAR0 = 0xFF; // ID28..ID21 are set

CANIDAR1 = 0xE6 | 0x18; // ID20..ID16 are set, plus IDE and SRR are set

 

Since all other bits (and probably RTR, you didn't say) are don't care, you don't have to set up CANIDAR2 and CANIDAR3.

 

Now masks.

CANIDMR0 = 0; // received ID28..ID21 have to match what's specified in IDAR0

CANIDMR1 = 1; // received ID20..ID16 (but not ID15), IDE, SRR have to match what's specified in IDAR1

CANIDMR2 = 0xFF; // ID14..ID7 are don't care

CANIDMR3 = 0xFF; // ID6..ID0 and RTR are don't care

0 Kudos
Reply
3,075 Views
francy
Contributor I
Thanks kef
0 Kudos
Reply