Bus-CAN parameters of configuration polling Identifier Register - MC9S08DZ60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bus-CAN parameters of configuration polling Identifier Register - MC9S08DZ60

1,985件の閲覧回数
esmiti
Contributor I
 In the microcontroller MC9S08DZ60 can be configured as the CAN-Bus to perform a scan (polling, etc) for know the ID's (Identifier Register) that are connected some devices? The use is to send a specific data to each one without having to develop a software? Thank you.
 
 
 
 
 
 
 
 
 
 
 
Added p/n to subject.
 


Message Edited by NLFSJ on 2009-02-05 11:16 AM
ラベル(1)
0 件の賞賛
返信
1 返信

971件の閲覧回数
Lundin
Senior Contributor IV
CAN bus identifiers are data-related, not device-related. It doesn't make sense to read an ID register of another CAN device.
0 件の賞賛
返信