Baud Rate and the MC9S080G8 uCtrl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Baud Rate and the MC9S080G8 uCtrl

4,692 Views
Cennedie
Contributor I
Im using the internal 16MHZ osc with the default ICS settings. 
My question is: "What speed does the BUSS run @ when using the Default 16Mhz clock?"
 
When looking thru the datasheet of the subject controller it shows three different things:
a) The internal frequency settings is nominally 16Mhz and will provide a 4Mhz BUSS out of a RESET.  (section 2.2.2, Oscilator section of datasheet)
 
b) The BUSS frequency will be 1/2 of the ICSOUT frequency (section 10.1, of datasheet)
 
c) The diagram shown in Figure 10.2 shows the ICSOUT signal being fed ny a 2^n divider, not a divide by two.
 
Can anyone help clear up my discrepencies,
 
Thanks
Brian
Labels (1)
0 Kudos
Reply
3 Replies

1,612 Views
peg
Senior Contributor IV

Hi Brian,

First I will presume you mean QG8,

Answer is 8MHz.

a.) Statement is WRONG!

b.) Statement is correct.

c.) Drawing is correct. The 2^n divider is controlled by BDIV which has a reset default of 01 which means /2.

Regards David

 

0 Kudos
Reply

1,612 Views
Alban
Senior Contributor II
Passed onto Datasheet owner
0 Kudos
Reply

1,612 Views
peg
Senior Contributor IV

Hi Brian,

My first response is WRONG!

The sections of the manual you refer to are ALL CORRECT!

The answer is 4MHz

For an explanation refer to Figure 10.2.

Start at the internal reference clock in the middle.
It runs at nominally 16MHz.
To IREFS.
IREFS defaults to 1 which selects internal rather than external clock.
Then through programmable divider controlled by RDIV.
RDIV defaults to 000 which is divide by 1. (16MHz)
Into the FLL.
CLKS defaults to 00 which selects the output of the FLL
then to another programmable divider controlled by BDIV.
BDIV defaults to 01 which is divide by 2. (8MHz)
Now the signal is called ICSOUT.
This is then divided by 2 to produce BUSCLK.(4MHz). (as noted in OP's b) section 10.1)

Sorry if I have lead anyone astray.

Alban, quick get that note to the datasheet owner back before he thinks we are all illiterate, especially me, then you and the 53 people that read my incorrect response without comment. :smileyvery-happy:

Regards David

 

Message Edited by peg on 2006-06-08 09:39 PM

0 Kudos
Reply