Basic IIC reading and writing between two 9S08's WITHOUT using interrupts.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Basic IIC reading and writing between two 9S08's WITHOUT using interrupts.

4,259件の閲覧回数
mcookfromwi
Contributor I
I have tried the "How to use the IIC module" as well as many other references but I seem unable to get IIC communications working between two 9S08's (one master addessed 0x11 and one slave addressed 0x33).  I am successful in having a MASTER send a slave ID (0x33) but the slave software does not send a ACK back.
 
Is IIC comms possible without using interrupts?  If so is there any examples I can try?
 
 
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,178件の閲覧回数
erooll
Contributor II
Could you show us, a piece of code that you are implementing.
Regards
0 件の賞賛
返信

2,178件の閲覧回数
mcookfromwi
Contributor I
The system seemed to loose my reply, this is my 2nd attempt.
 
/////////////////////////////////////////////////////////////
// Init_I2C
//  sets up the iic port according to the state
//    selfAddress = slave address
//   
void Init_I2C (unsigned char selfAddress)
{   
    SOPT2_IICPS = 1; //Set the IICPS bit  to redirect IIc pins   
    IICC_IICEN = 1;//Enable IIC module
    IICC_TXAK = 1;// SEND ACK 
    IICC_MST = 0;//SLAVE MODE     
    IICA = selfAddress << 1;//set slave address in IICA  //PTB6=SDA PTB7=SCL
   
    //set baud rate = BUSCLK/(2xMULTx(SCL Divider))
    //     MUX | ICR|
    //      \\  /////       
    IICF = 0b10010000;//MUX=2,ICR=0x16 Speed=100Khz
                         
       
    IICS_SRW = 0;//R/W bit  = 0
    IICC_IICIE = 0;//Disable IIC interrupt           
    
}
 
//////////////////////////////////////////////////////////////////////////////////
// IIC_write_byte
//    Writes command and data to slave
//   returns 0 if success
//           1 if error
byte IIC_write_byte (byte slave, byte command, byte data)
{
   byte temp;
   byte timeout = 0xFF;
   temp = (slave)<<1;     // Shift 7 bit slave address to the left 1 bit
                          // Bit 0 = 0 = Write
                          //     0 = 1 = Read
   IICC_TXAK = 0;         // RX/TX = 1;  MS/SL = 1; TXAK = 0;
   IICC |= 0x30;          // Generate START & set TX = 1
  
   IICD = temp;           // select slave & set up for master transmit
   while (!IICS_IICIF);   // wait until flag is set
   IICS_IICIF=1;          // Clear the flag
   while((IICS_RXAK)&&(timeout > 0))
      timeout --;      // check for RXAK
   if(timeout == 0) return 1;
   IICD = command;        // Send byte address
   while (!IICS_IICIF);   // wait until flag is set
   IICS_IICIF=1;          // Clear the flag
   //while(IICS_RXAK);      // check for RXAK
   timeout = 0xFF;
   while((IICS_RXAK)&&(timeout > 0))
      timeout --;      // check for RXAK
   if(timeout == 0) return 1;
   IICD = data;
   while (!IICS_IICIF);   // wait until flag is set
   IICS_IICIF=1;          // Clear the flag
   //while(IICS_RXAK);      // check for RXAK
   timeout = 0xFF;
   while((IICS_RXAK)&&(timeout > 0))
      timeout --;      // check for RXAK
   if(timeout == 0) return 1;
   IICS_IICIF=1;          // Clear the flag
   IICC_MST = 0;          // Generate STOP
   return 0;
}
  
//////////////////////////////////////////////////////////////////////////////////
//  IIC_read_byte
//    Writes command to slave and returns data from slave
//   returns 0 if success
//           1 if error
byte IIC_read_byte (byte slave, byte command)
{
   byte RD_data;
   byte temp;
   temp = (slave)<<1;     // Shift 7 bit slave address to the left 1 bit
                          // Lsb Bit = 0 = Write
                          //         = 1 = Read
   IICC_TXAK = 0;
   IICC |= 0x30;          // Generate START
   IICD = temp;           // Address slave | (RW = 0), write to slave
   while (!IICS_IICIF);   // wait until flag is set
   IICS_IICIF=1;          // Clear the int flag
   while(IICS_RXAK);      // Check for RXAK
   IICD = command;        // Send command to slave
   while (!IICS_IICIF);   // wait until flag is set
   IICS_IICIF=1;          // Clear the int flag
   while(IICS_RXAK);      // Check for RXAK
   IICC_RSTA = 1;         // setup repeated start
   IICD = temp|1;         // (slave_address)|(RW = 1), read from slave
   while (!IICS_IICIF);   // wait until flag is set
   IICS_IICIF=1;          // Clear the int flag
   while(IICS_RXAK);      // Check for RXAK
     
   IICC_TX = 0;           // Setup to receive
   IICC_TXAK = 1;         // Acknowledge disable
   RD_data = IICD;        // Dummy read
   while (!IICS_IICIF);   // Wait until IBIF flag is set
   IICS_IICIF=1;          // Clear the flag
   IICC_MST = 0;          // Generate STOP
   RD_data = IICD;        // Read data
   return RD_data;
}
 
[[[Below is ione of my attempts at the slave read routine]]]
 
/////////////////////////////////////////////////////////////
// LL_Read()
byte LL_Read()
{     
   //ToggleNum(0x33);
   //return 0x33;
   //IICC_TX = 0; 
   //IICC_TXAK = 0;         // Acknowledge enable
   //IICS_IICIF=1;
   //IICC_MST = 0;//SLAVE MODE  
   //while(IICS_TCF == 0)      
   //   ToggleNum(IICS);
   if(IICS_IAAS)
   {
      IICC_TX = IICS_SRW;  //SRW 0= slave receive, 1=slave transmit
      IICS_IAAS = 0;       // Setup to receive  
       buffer[0] = IICD;      // Dummy read to initiate the read data byte
       buffer[1] = IICD;
       return 1;
   }
   //RD_data2 = IICD;         //read data
   //IICS_IICIF=1;           //Clear the flag
   //IICC_MST = 0;         //Generate STOP
   return 0;       
}
0 件の賞賛
返信

2,178件の閲覧回数
Designer11
Contributor IV
Hi,

what method are you using to maintain the IIC communication, interrupt or polling ?
0 件の賞賛
返信