AN2295 for MC9S08AW32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN2295 for MC9S08AW32

1,454 Views
oskaratk
Contributor I

hi .. I am fairly new to the world of microchips, so please excuse all my questions.

Managed to my app working using  PeMicro Multilink ...  however  

 

now I am trying to figure how AN2295 bootloader works with a MC9S08AW32 MCU. Trying to use single wire

 

Into the AN2295 docu, the only reference to this MCU I am finding in Table 2, so I assume I have to use FC protocol V3.

But when I load the project hc08sprg-s08aw.mcp  from the S08AW folder .. that is using FC protocol V2.

 

I have compiled loaded aboutve project and flashed.

 

running hc08sprg com1:smileyfrustrated: 9600 mys19.s19, after a powerdown reset, I am getting :

 

Waiting for HC(s)08 reset ACK ... received 0xdc (good)

Calibration break pulse sent. Count: ....

 

seem to be stuch in that loop counting.

 

I seem to see the break at RDX1 of the MCU

 

 

Any help is highly appreciated

 

Thanks

Oskar

Labels (1)
0 Kudos
Reply
1 Reply

1,135 Views
oskaratk
Contributor I

well, I found my problem:

 

BEWARE of some USB to serial converters/cables.

 

Using a PC with a real RS232 port helped ... then I found a working USB-Serial cable too ...

 

Now the bootloader works just out of the box

 

Oskar

0 Kudos
Reply