AN2295 - Store a few byte in protected memory ( Serial Number)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN2295 - Store a few byte in protected memory ( Serial Number)

1,521 次查看
oskaratk
Contributor I

Hi,

 

I am using the serial bootloader to flash my app to a MC9S08AW32 . Works like perfect.

 

However, now I have the request to store a serial number in protected memory - just 2 or 4 bytes would be plenty.

My understanding is that the bootloader sets the flash protectioin flags to protect itself - So I would need to "issue" and flash the serial number when the bootloader itself is initially flashed, correct ?

Which in turn would require to modify the bootloader code and memory layout ?

 

Are my thoughts remotely correct? Any hints are highly appreciated

 

( Coming from the win32 world ... dealing with bits and bytes is not that esy for me )

 

Thanks

Oskar

标签 (1)
0 项奖励
回复
1 回复

1,283 次查看
Mickey
Contributor III

Hi P&E cyclonepro have program serial number function. for you information.

0 项奖励
回复