ADC resolution on the DEMOJM board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC resolution on the DEMOJM board

1,630 Views
johnpaul013
Contributor I

I have an accelerometer attached to the ADC chip on my DEMOJM board.

The ADC chip can be set for 8, 10, or 12 bit resolution.

However, when I set it for 12-bit resolution, I only see 11 bit values.

I would expect  to see raw A/D counts go from 0 - 4095.

Instead, I see the counts go from 0 - 2047.

Anybody have any ideas?

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,255 Views
Betadine
Contributor III

Hi John,

Im not an expert but I have been dealing with the JM DemoBoard and the ADC.

The first place where I would look -> initiliazing the ADC.

Take the datasheet and look for every flag in the init process.

 

Also take a look in the code (I get mad with the DemoJM Examples) but you will finally understand it by some way

 

Have you seen the voltages in the ADC pins? Make sure you have 5Vcc... ...  but as you say ...2047 is exactly the half of 4095, so I think that the hardware is not the problem.

 

I found some C examples from the internet "search for nikola" for this demoboard, using the ADC, not bad for understand how theADC works.

 

Hope it helps

 

 

 

 

 

0 Kudos
Reply