9S08AW32 Newbie Question - Where to Start

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

9S08AW32 Newbie Question - Where to Start

1,752 次查看
Jack8421
Contributor I

Hi All,

 

I'm an electronics engineer by day and an enthusiast veteran Atmel AVR assembler programmer in my spare time. I'd like to master 9S08AW micros and have a couple of questions which you might be kind enough to help with:

 

1.  Is the following the correct development software for 9S08AW assembler coding ?

     CodeWarrior™ Development Studio for Microcontrollers V6.3

 

2.  Which is the cheapest programming hardware for 9S08AW ?

 

Many thanks

标签 (1)
0 项奖励
回复
2 回复数

1,575 次查看
bigmac
Specialist III

Hello, and welcome to the forum.

 

For non-automotive use, you might use the later MC9S08AC family, rather than the 'AW series.

 

You might also consider purchasing a demonstration board that already has an on-board USB multilink interface for programming and debug.  The demonstration board is also fitted with a 64-pin socket for the MCU device.  By removal of the onboard device, and the fitting of a suitable lead, external programming and debug is possible.

 

Regards,

Mac

 

0 项奖励
回复

1,575 次查看
raining
Contributor I
0 项奖励
回复