908GP32 - Address issue - pointer in C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

908GP32 - Address issue - pointer in C

2,783件の閲覧回数
Stefano_RadioLa
Contributor I
Hi,
I am programmind 908GP32 with codewarrior usign C.
I have this question: i have a variable ( int not a pointer) and a data structure (array of int)
How can I do the following operation?

myvariable=address data structure

I need this because I am trying to implent a eeprom using flash with the driver descripted in an3040.      

Do you have some suggestion?

Tx

--
Alban Edit: Changed title: Part number must be shown and clarified subject.



Message Edited by Alban on 2007-06-07 11:36 AM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,510件の閲覧回数
thisobj
Contributor III
Hello Stefano,
You'll need to cast the address value to an "int" type to avoid a type mis-match error. 
The following should work:

int myvariable;

int somearray[2];

void main(void) {

myvariable = (int)(&somearray);

// now to use "myvariable" as a pointer....

*(  (int *)myvariable ) = 20;      // places "20" at somearray[0];

}

Note that using pointers that are built by casting can lead to very difficult-to-find bugs.  This usually occurs when incrementing or decrementing the pointer.

Frank


0 件の賞賛
返信

1,510件の閲覧回数
Alban
Senior Contributor II
Hello,

& is the operator for address:

myvariable = &DataStruct;


Cheers,
Alban.
0 件の賞賛
返信