8 BIT Math Reference Guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8 BIT Math Reference Guide

4,093 Views
BobMac
Contributor I
Is there a good basic reference publication for 8 BIT math with HC908 devices?
Regards, BobMac
Labels (1)
0 Kudos
Reply
3 Replies

1,847 Views
peg
Senior Contributor IV
Hi Bobmac,
 
AN1219 is all that I know of.
 
Regards
David
 
0 Kudos
Reply

1,847 Views
bigmac
Specialist III
Hello BobMac,
 
Not quite sure what you require here.
 
AN1219 covers some multiple byte integer routines.  The operating details of all instructions, including the math(s) ones, are covered by the document CPU08RM.  This also includes example code for some of the less familiar instructions.
 
Regards,
Mac (another one)
 
0 Kudos
Reply

1,847 Views
BobMac
Contributor I
Well, Hi everybody!

I was looking for a book on basic computer 8 bit math that I could use for reference. I was quite good at this in the early '70s 6502, 6809 'hc11 etc but haven't used this skill for quite a while. Let's see, 76- 86, 96, 2006. Yup, that's about 25 year's of dying brain cells ;o).
Any hot tips would be most welcome.
Regards, Bob
0 Kudos
Reply