13192-SARD - Can you teach me about Beacon Tree Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

13192-SARD - Can you teach me about Beacon Tree Mode

12,473件の閲覧回数
insider
Contributor II
Hi, Spell. I'm andershen. Currently, I'm dealing with 13192-SARD boards. I plan to form a tree network using MAC codebase example project, MyStarNetwork. In BeeKit, it only provides coordinator and end device example. How do we create a router?
 
Thanks.
 
Best wishes,
andershen

--
Alban Edit: FSL Part Number in Subject line + split/moved to appropriate location.



Message Edited by Alban on 2007-09-03 09:11 PM
ラベル(1)
0 件の賞賛
返信
23 返答(返信)

774件の閲覧回数
insider
Contributor II
Hi, spell. I still have problem with the router. Any suggetion of making a router using the MAC codebase?
Sorry for the inconvenient.
0 件の賞賛
返信

774件の閲覧回数
Spell
Contributor I
Hi insider,
which kind of problem do you have?
Try to download the ZR_CustomApp that I have attached in page 1 and take a look to it.

Regards, Filippo
0 件の賞賛
返信

774件の閲覧回数
Spell
Contributor I


insider wrote:
you gave me the program is for 13213, is it suitable for 13192-SARD board?


Make a new project with beekit for your board and then change the MApp.c file with the new one. :smileywink:
0 件の賞賛
返信