Is ODT(on-die termination) not necessary for T topology?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is ODT(on-die termination) not necessary for T topology?

1,529 Views
王剑翰
Contributor III

In IMX6SLHDG.pdf, Page 30:

2.5.2 DDR3 (32 bits) T topology considerations

Be sure to take into account the following when designing a T-topology system.

• Follow the routing rules described in  Table 2-3 .

• Termination resistors not required.

• Short routing lengths and on -chip drive strength control.

• Your design is limited to 4 DDR chips.

• DDR3, 2 GBytes using latest memories (4 GBytes coming).

As above claimed,  termination resistors is not necessary for T topology. So ODT is NOT required for T topology? I can not understand it. Please kindly explain it or correct me if my understanding is wrong. Thank you!

Labels (3)
0 Kudos
Reply
2 Replies

1,266 Views
王剑翰
Contributor III

I have got the answer.

0 Kudos
Reply

1,266 Views
jamesbone
NXP TechSupport
NXP TechSupport

OK, so we are closing your question.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply