I want to know that how can i use 68332 code on CodeWarrior 68K software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to know that how can i use 68332 code on CodeWarrior 68K software

1,276 Views
ivanzhang
Contributor II

Dear:
      excuse me . Our company buy the CodeWarrior 68K  software to code on 68332,but i don't know how to use 68332 code on this software and  i dont know how to creat 68332 project, Is it same as 68360?  If it is convenient for you, send me the 68332 sample project , please,thank you very much .   my email Add: 422518623@qq.com

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,145 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Sorry, there is no such example available for m68332.
You can use the project wizard to create a project for 68360 and adapt it for 68332 for this purpose.
Sorry for the inconvenience.

The current version for 68k is the CodeWarrior for 68k V3.2.

CodeWarrior® Development Tools for 68K|NXP 


- Stationery and examples support for the following processors are no longer included: MC5206eLite, MC68328ADS, MC68EZ328ADSv1, M68332EVS.
I checked on the old installation and found an 68332 stationnery under the V2.0.
This is a very old tool version released in 2000.
I don't know if the example will work on the V3.2.
Excepted this example we don't have other one.

Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply