MMC: no card present custom IMX6 UL Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMC: no card present custom IMX6 UL Board

8,621 Views
nachodiz
Contributor III

Dear all

Our board is succesfully booting from SD1

But UBOOT says MMC: no card present

Sometimes it detects the card  mmc0 is current device

But the major of the times its not being detected

We have no physical (mechanical card detect)

How can we fix the issue ?

King Regards

eee.png

Labels (1)
0 Kudos
Reply
7 Replies

6,135 Views
Yuri
NXP Employee
NXP Employee

Hello,

  First, as I see from boot log, PMIC is not defined in U-boot.

It should be defined in U-boot with following rebuild.

You may look at “[PATCH] u-boot: add pf3000 support on imx6ul-14x14-evk board”

 

 To support eMMC it is needed to rebuild U-boot ; please refer to

section 5.5 (U-Boot configuration) of “i.MX_Yocto_Project_User's_Guide.pdf”.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply

6,135 Views
nachodiz
Contributor III

We are workind from sd card (sd1)
boards are fused to boot from sd card sd1 bus
emmc is at sd2


the evk has card detect on sd1
mechanical
i think this is our problem
we have no mechanical card detect

it boots from sd1
but uboot is not seeing sd1

0 Kudos
Reply

6,135 Views
nachodiz
Contributor III

Some times it boots!


U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (May 05 2017 - 15:16:44 +0300)

CPU:   Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 45C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C:   ready
DRAM:  512 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc0 is current device
Net:   FEC1
Error: FEC1 address not set.

Normal Boot
Hit any key to stop autoboot:  0
=> boot
switch to partitions #0, OK
mmc0 is current device
switch to partitions #0, OK
mmc0 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
6635592 bytes read in 297 ms (21.3 MiB/s)
Booting from mmc ...
reading imx6ul-14x14-evk.dtb
36042 bytes read in 18 ms (1.9 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x654048 ]
## Flattened Device Tree blob at 83000000
   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 83000000, end 8300bcc9
Modify /soc/aips-bus@02000000/bee@02044000:status disabled
ft_system_setup for mx6

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.1.15-2.0.1+gb63f3f5 (yaroslav@ux330uak) (gcc version 5.3.0 (GCC) ) #1 SMP PREEMPT Fri May 5 13:59:24 MSK 2017
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8bb32000 s16908 r8192 d24052 u49152
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 178620K/524288K available (8359K kernel code, 433K rwdata, 2944K rodata, 432K init, 449K bss, 17988K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xa0800000 - 0xff000000   (1512 MB)
    lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x80b11ea4   (11304 kB)
      .init : 0x80b12000 - 0x80b7e000   ( 432 kB)
      .data : 0x80b7e000 - 0x80bea5a0   ( 434 kB)
       .bss : 0x80bed000 - 0x80c5d540   ( 450 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
        Additional per-CPU info printed with stalls.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
mxc_clocksource_init 24000000
Switching to timer-based delay loop, resolution 41ns
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80008280 - 0x800082d8
Brought up 1 CPUs
SMP: Total of 1 processors activated (48.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.20
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
MIPI DSI driver module loaded
MIPI DSI driver module loaded
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 60x34
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed
spi_gpio spi4: gpio-miso property not found, switching to no-rx mode
CAN device driver interface
flexcan 2090000.can: device registered (reg_base=a09e8000, irq=28)
flexcan 2094000.can: device registered (reg_base=a09f0000, irq=29)
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 3a:57:55:56:26:d2
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 6a:74:bd:4b:cb:4f
fec 2188000.ethernet eth1: registered PHC device 1
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1
read sensor who am i (0xfffffffb)error !
fxls8471: probe of 0-001e failed with error -22
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
0-000e supply vdd not found, using dummy regulator
0-000e supply vddio not found, using dummy regulator
mag3110 0-000e: check mag3110 chip ID
mag3110 0-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 0-000e failed with error -22
imx2-wdt 20bc000.wdog: use WDOG_B to reboot.
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
caam 2140000.caam: Entropy delay = 3200
caam 2140000.caam: Instantiated RNG4 SH0
mmc1: MAN_BKOPS_EN bit is not set
caam 2140000.caam: Instantiated RNG4 SH1
caam 2140000.caam: device ID = 0x0a16030000000000 (Era -524)
caam 2140000.caam: job rings = 3, qi = 0
mmc1: new DDR MMC card at address 0001
mmcblk1: mmc1:0001 004GE0 3.68 GiB
mmcblk1boot0: mmc1:0001 004GE0 partition 1 2.00 MiB
mmcblk1boot1: mmc1:0001 004GE0 partition 2 2.00 MiB
mmcblk1rpmb: mmc1:0001 004GE0 partition 3 512 KiB
caam algorithms registered in /proc/crypto
caam_jr 2141000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 8 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] e0 5a 42 a9 3a b8 27 2f
platform caam_sm: [0008] 2a 7a 00 39 d6 8e 5f 95
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 49 ca 71 36 08 03 90 6a
platform caam_sm: [0008] c6 17 a1 1e d0 b1 39 84
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] f1 cf e3 19 43 a8 aa ef
platform caam_sm: [0008] 56 b4 57 8c 65 59 e6 7d
platform caam_sm: [0016] 77 5a 86 14 98 fa 7b c4
platform caam_sm: [0024] c6 fa a0 a2 14 b7 ad 3b
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 8f 78 43 33 17 19 51 ee
platform caam_sm: [0008] 4e 35 a6 e5 6f fc 70 d8
platform caam_sm: [0016] 42 25 8b 07 0e 0f cb d2
platform caam_sm: [0024] 0e e4 93 47 98 99 47 49
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 2c db 2b 1b 2c 8b 23 c0
platform caam_sm: [0008] b6 7f b4 f2 54 d4 2a c1
platform caam_sm: [0016] 47 4d b6 d1 e9 fd ae 8e
platform caam_sm: [0024] be c5 2e cb 1c 97 ab d7
platform caam_sm: [0032] cb 8d 8f 12 cc 8d 80 9a
platform caam_sm: [0040] 2b d0 d1 9b 89 a9 c2 2d
platform caam_sm: [0048] 85 f2 f3 f2 9a 43 46 cd
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 9b f2 d2 64 6a 26 a9 3e
platform caam_sm: [0008] 52 16 06 6f 19 d5 17 5f
platform caam_sm: [0016] b2 b3 92 7f 9c b6 55 4d
platform caam_sm: [0024] f8 1f 13 f9 9f bb c1 cf
platform caam_sm: [0032] d0 0a 0c 39 a6 0f f2 8b
platform caam_sm: [0040] c6 36 25 a4 71 20 fd 5f
platform caam_sm: [0048] dd b0 8c 78 66 39 29 e1
platform caam_sm: [0056] e0 b5 4c 11 44 25 ff 5e
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 0f 99 17 6c 85 f6 fc 73
platform caam_sm: [0008] a2 15 21 9d 7c 86 80 c2
platform caam_sm: [0016] 2d 3d 87 04 91 b3 53 3a
platform caam_sm: [0024] 93 4d 18 72 4e 08 47 f7
platform caam_sm: [0032] 96 45 69 f2 ca 4c 6f 35
platform caam_sm: [0040] e5 2d 3c 90 2d dd 4f f1
platform caam_sm: [0048] 50 2c 01 a5 51 6d bc 3d
platform caam_sm: [0056] e3 aa 8d 8e 89 75 e0 e5
platform caam_sm: [0064] 39 20 52 fe 26 0e 2c 8c
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 65 90 7d ee 9a bc da 11
platform caam_sm: [0008] 59 8d fa 74 89 83 3c 94
platform caam_sm: [0016] 08 ce e5 69 9d 79 0b 35
platform caam_sm: [0024] bf 2c ef fa 8e d1 c1 af
platform caam_sm: [0032] e1 e0 20 d7 80 dd 50 a8
platform caam_sm: [0040] 98 cf 72 24 d8 f4 48 30
platform caam_sm: [0048] 24 9c b1 b3 f1 6d 8e e3
platform caam_sm: [0056] 75 47 8d 17 1c 05 28 41
platform caam_sm: [0064] 31 c1 70 0d bb 24 f5 c6
platform caam_sm: [0072] 00 58 4f 94 7f 2b 9f 48
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] bb ef d0 7a eb e9 09 41
platform caam_sm: [0008] 40 20 af 31 c6 4f 0f 0d
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 49 ca 71 36 08 03 90 6a
platform caam_sm: [0008] c6 17 a1 1e d0 b1 39 84
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] f1 cf e3 19 43 a8 aa ef
platform caam_sm: [0008] 56 b4 57 8c 65 59 e6 7d
platform caam_sm: [0016] 1a 52 17 cf dc 6e 94 f7
platform caam_sm: [0024] f1 66 aa 99 5e ed b6 29
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 8f 78 43 33 17 19 51 ee
platform caam_sm: [0008] 4e 35 a6 e5 6f fc 70 d8
platform caam_sm: [0016] 42 25 8b 07 0e 0f cb d2
platform caam_sm: [0024] 0e e4 93 47 98 99 47 49
snvs-secvio 20cc000.caam-snvs: can't get snvs clock
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8960 1-001a: Failed to issue reset
wm8960: probe of 1-001a failed with error -5
fsl-asrc 2034000.asrc: driver registered
imx-wm8960 sound: failed to find codec platform device
imx-wm8960: probe of sound failed with error -22
NET: Registered protocol family 26
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
dhd_module_init in
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
gpio_dvfs: disabling
VSD_3V3: disabling
can-3v3: disabling
ALSA device list:
  No soundcards found.
Waiting for root device /dev/mmcblk0p2...

0 Kudos
Reply

6,135 Views
nachodiz
Contributor III

But stil hangs

Waiting for root device /dev/mmcblk0p2...


0 Kudos
Reply

6,135 Views
Yuri
NXP Employee
NXP Employee

Hello,

  is Your memory settings in U-boot just the same as for DDR stress test

(with taking into account results of calibration) ?

You may try to set SD1_CD active for testing.

Regards,

Yuri.

0 Kudos
Reply

6,135 Views
nachodiz
Contributor III

No its not ...


0 Kudos
Reply

6,134 Views
Yuri
NXP Employee
NXP Employee

1.

   You may try to set SD1_CD active for testing.

2.

  To avoid memory issues - please provide correct initialization in U-boot 

(Please refer to U-boot chapter in "i.MX_BSP_Porting_Guide.pdf").

DRAM Customization on i.MX6x | NXP Community 

~Yuri.

0 Kudos
Reply