powerpc-eabivle.gdb.exe crashes during debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

powerpc-eabivle.gdb.exe crashes during debug

5,085件の閲覧回数
ronlewis
Contributor III

I am having issue debugging an application.  powerpc-eabivle.gdb.exe crashes while connecting to the MPC5644a.  Its only an issue on the one project, and will occasionally work.

IE: I can debug other projects without issue, but for one project it mostly fails and I can get it to connect occasionally.  I have compared the debugger settings and I don't see any differences.  

Has anyone seen this issue?  Any guidance?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

4,595件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Ron,

Could you possibly try to update Pemicro e200 debugging support plugin?

It includes some new features + some bug fixes.

See the instructions here: https://community.nxp.com/message/890477?commentID=890477#comment-890477 

Just select "GNU E200 PEMicro Interface Debugging Support" instead of ARM one

Please let us know it it helps.

Thanks!

Stan

0 件の賞賛
返信

4,595件の閲覧回数
ronlewis
Contributor III

The support plugins where already up to date.  I ended up creating a new project and coping the source files over to the new project and that fixed the issue.

0 件の賞賛
返信