Boot up sequence of i.MX6UL through eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot up sequence of i.MX6UL through eMMC

1,445 Views
surendrajadhav
Contributor IV

Hi,

Can any one tell me the the BOOT_CFG setting for configuring the boot through eMMC.

Following configuration I tried to have booting from eMMC. Kindly confirm or suggest the seeting of Boot_CFG.

Booting.PNG

Red numbers shows my setting where 1 represents Pull up and 0 represents Pull down.

Regards,

Surendra

Labels (1)
0 Kudos
Reply
1 Reply

1,302 Views
igorpadykov
NXP Employee
NXP Employee

Hi Surendra

I think settings are correct, note also bus width should be configured in eMMC

Extend CSD register byte[177] bit[0:1].

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply