CW 10.1 on MCF5225X TWR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.1 on MCF5225X TWR

2,091 Views
yuxing
Contributor I

Hi there, 

 

I recently migrated to Freescale tower system. 

 

Old environment: MCF5211DEMO board in CodeWarriror 5.7.0 

Current environment: TWR with MCF5225X in CodeWarrior 10.1

 

In the old dev environment when a new project is created, CodeWarrior would have a set of support files available, like mcf5xxx.c, mcf5xxx_lo.s, which contains a bunch of handy support functions like cpu_pause(), asm_set_ipl(), mcf5xxx_set_handler(), etc.  

 

But with CW10.1 there is no more such functions. So my question is, are there any similar files/functions/lib that are available in CW10.1? Is so, how can I find them? I do have the source code from old projects so I assume copying them over could solve my problem, but I would like to have CW10.1 make it a default bundle when creating new projects. Can anyone help please?

 

Thanks in advance.

Labels (1)
0 Kudos
Reply
2 Replies

1,831 Views
CamiloA_
Contributor III

I have the same problem using USB CMX stack on CW10.

0 Kudos
Reply

1,831 Views
BlackNight
NXP Employee
NXP Employee

I have solved the problem for myself with having such files part of my project.

 

BK

0 Kudos
Reply