LPCXpresso IDE error: cannot find -llpc_board_nxp_lpcxpresso_824

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso IDE error: cannot find -llpc_board_nxp_lpcxpresso_824

2,199件の閲覧回数
enzoguerra
Contributor I

trying to use LPCXpresso IDE

followed tutorials best i could

imported lpcopen_2_19_lpcxpresso_nxp_lpcxpresso_824.zip

did simple build all command

got +100s of errors

many misspellings, etc...

but one of the errors on all projects was: cannot find -llpc_board_nxp_lpcxpresso_824

found the project: lpc_board_nxp_lpcxpresso_824, has no makefile

also found, all the project \Debug\example\src has the file subdir.mk which has the lines:

# Each subdirectory must supply rules for building sources it contributes
example/src/%.o: ../example/src/%.c
    @echo 'Building file: $<'
    @echo 'Invoking: MCU C Compiler'
    arm-none-eabi-gcc -DDEBUG -D__CODE_RED -D__USE_LPCOPEN -D__MTB_BUFFER_SIZE=128 -D__REDLIB__ -DCORE_M0PLUS -I"C:\Users\enzo_\Documents\LPCXpresso_8.2.0_647\workspace\lpc_chip_82x\inc" -I"C:\Users\enzo_\Documents\LPCXpresso_8.2.0_647\workspace\lpc_board_nxp_lpcxpresso_824\inc" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m0 -mthumb -specs=redlib.specs -MMD -MP -MF"$(@:%.o=%.d)" -MT"$(@:%.o=%.o)" -MT"$(@:%.o=%.d)" -o "$@" "$<"
    @echo 'Finished building: $<'
    @echo ' '

can someone help, i not to sure what to do

also got other errors:

make: *** [freertos_blinky.axf] Error 1

and many more with:

make: *** [xxx.axf] Error 1

where xxx is the project name

except for periph_blinky which has this error:

make: *** [example/src/sysinit.o] Error 1

the similar subdir.mk which has the lines:

# Each subdirectory must supply rules for building sources it contributes
example/src/%.o: ../example/src/%.c
    @echo 'Building file: $<'
    @echo 'Invoking: MCU C Compiler'
    arm-none-eabi-gcc -D__REDLIB__ -O0 -g3 -Wall -c -fmessage-length=0 -mcpu=cortex-m0 -mthumb -D__REDLIB__ -specs=redlib.specs -MMD -MP -MF"$(@:%.o=%.d)" -MT"$(@:%.o=%.o)" -MT"$(@:%.o=%.d)" -o "$@" "$<"
    @echo 'Finished building: $<'
    @echo ' '

thanks

enzo

0 件の賞賛
返信
2 返答(返信)

1,695件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

I suggest that you restart the IDE in a completely new workspace.

Then use the Quickstart -> Import Project(s) -> Archive option and browse to the LPCOpen ZIP file for 824 in the LPCXpresso Examples subdirectory. Having selected this click on "Finish" to import all the projects from the ZIP.

Once everything has import, highlight "periph_blinky" project in the Project Explorer view (top left of the IDE window), then click on the "Build 'periph_blinky' [Debug]" button that should be visible in the Quickstart Panel.

Hopefully, the blinky project should then successfully build.

For more help, read the supplied LPCXpresso IDE User Guide, or view the videos at http://www.nxp.com/lpcxpresso

If you still have problems, then the below FAQ might also provide some additional hints.

Linker Error "cannot find -l&lt;lib_name&gt;" 

Regards,

LPCXpresso Support

0 件の賞賛
返信

1,695件の閲覧回数
enzoguerra
Contributor I

hello

thanks for reply

yes, already did that and everything seems to work

reviewing the lpcxpresso tutorials helped, must have missed something

regards

enzo

0 件の賞賛
返信