Does imx-android-l5.1.1_2.1.0-ga support DRM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does imx-android-l5.1.1_2.1.0-ga support DRM?

2,137 次查看
calvinyu
Contributor II

Hi

We have a project which uses iMx6 Quad and Android 5.1.

The BSP version is imx-android-l5.1.1_2.1.0-ga.

There are 2 questions.

1. Does the imx-android-l5.1.1_2.1.0-ga BSP support DRM feature?

2. How to write the DRM key to the device ?The DRM key is from google.

B.R

Calvin

0 项奖励
回复
3 回复数

1,683 次查看
pratik0403
Contributor I

Hi,

 

I have couple of questions with the same Widevine compliance on Android.

1. Is "Widevine level 1 compliance for DRM" implemented/available for IMX6 on Android platform? or Do we need to purchase separately?

2. If it is already implemented, then where we can find it's relevant document?

 

Thanks & Regards,

Pratik

0 项奖励
回复

1,683 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Calvin

it is supported as separate patch (not included in default

Android release), note customer needs license with google,

please contact local marketing for that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,683 次查看
calvinyu
Contributor II

Hi igor

Thank you for your information.

0 项奖励
回复