I want to use H264codes,but the frame data is in YCbCr 4:2:2 format. Do I need to translate it from YCbCr 4:2:2 to YCbCr 4:2:0 first?
I have seen the demo mxc_vpu_text.
in struct frame_buf *framebuf_alloc(int stdMode, int format, int strideY, int height, int mvCol) function,there is
fb->addrY = fb->desc.phy_addr; | |
fb->addrCb = fb->addrY + strideY * height; | |
fb->addrCr = fb->addrCb + strideY / divX * height / divY; | |
fb->strideY = strideY; | |
fb->strideC = strideY / divX; |
it means that the demo is only favor of planar format, not packed format, am i right?
thank you very much.
解決済! 解決策の投稿を見る。
Hi dongming
it is not necessary to translate it from YCbCr 4:2:2 to YCbCr 4:2:0,
but provide a 4:2:0 or 4:2:2 vertical formatted input YUV image with a
pre-defined size. Please refer to sect.4.2.3.1 YUV Input Loading
attached VPU Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi dongming
it is not necessary to translate it from YCbCr 4:2:2 to YCbCr 4:2:0,
but provide a 4:2:0 or 4:2:2 vertical formatted input YUV image with a
pre-defined size. Please refer to sect.4.2.3.1 YUV Input Loading
attached VPU Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
ok,thank you. But i cannot find YUV Input Loading attached VPU Manual. Could you please offer it?
attached doc will appear some time later (seems system is scanning it
for viruses), still you can find this document in BSP package
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)
~igor