GSM fecility on sabresd board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GSM fecility on sabresd board

2,151 Views
sachusanal
Contributor III

Hai Sir ,

I have imx6qsabresd  evaluation kit with me. I flashed the lolipop android prebuilt image on sabresd board. i found that in board there is one CON1-SIM card connector .

i put one sim on that port  if this board have GSM fecility for calling /not? otherwise it only support messaging ? in android OS i found only messaging option .

how can i check this one.

Labels (1)
0 Kudos
Reply
1 Reply

2,053 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sachu

SIM can be accessed using AT commands, also

3G modem Huawei EM770W is supported in Android

(refer to attached Release Notes p.4):

Re: SIM card Connector port sabresd board reg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply