imx.6 SABRESD with mag3110

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx.6 SABRESD with mag3110

1,762 Views
bottleneck
Contributor III

Hi,

I am using SABRESD board, is anyone successful in using mag3110 magnetometer. Does it required to do any rework on the board.

Does anyone share the I2C Master configuration values to get acknowledgement from mag3110. Can anyone share the pad and mux

configuration for mag3110 on I2C3. Please do needful

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,544 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I have tried the fsl-image-gui image generate in Yocto.

This one contains the evtest-capture program that you can use to test the magnetometer.

Also you can check the configuration in the imx6qdl-sabresd.dtsi file, like the i2c port used and the gpio pin used for the irq.

Best Regards,

Alejandro

0 Kudos
Reply