what is the best way for Timeout on UART RX with MQX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the best way for Timeout on UART RX with MQX?

4,908 Views
holyhope
Contributor III

Hi to all,

I have develop (with support of another user of this community) an UART RX with demo board FRDM-K64 with MQX 4.1.1 using KDS 1.1.1

Now the code is that:

main.c:

#include <mqx.h>

#include <bsp.h>

#include <sem.h>

#include "main.h"

#if ! BSPCFG_ENABLE_IO_SUBSYSTEM

#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.

#endif

#ifndef BSP_DEFAULT_IO_CHANNEL_DEFINED

#error This application requires BSP_DEFAULT_IO_CHANNEL to be not NULL. Please set corresponding BSPCFG_ENABLE_TTYx to non-zero in user_config.h and recompile BSP with this option.

#endif

#define MaxSci1_CHANNEL "ittyb:"

LWSEM_STRUCT    lwsemUartRX;

typedef struct rx_str_template

{

  char data_buf_RX[256];

  _mqx_uint nCharRx;

  _mqx_uint ConteggioInternoCharRicevuti;

} RX_STR, * RX_STR_PTR;

RX_STR rx_str;

void main_task (uint32_t initial_data){

   _task_id   task_id;

   uint32_t result;

   result = _lwsem_create(&lwsemUartRX, 0);

   if (result != MQX_OK) {

       printf("\nCreating lwsemUartRX failed: 0x%X", result);

       _task_block();

   }

   task_id = _task_create(0,READ_TASK, 0);

   printf("\nread_task created, id 0x%lX", task_id);

   while(1)

   {

    _lwsem_wait(&lwsemUartRX);

    printf("\nData:\n ");

    int i =0;

    for(i=0;i<rx_str.nCharRx;i++){

    printf("%c",rx_str.data_buf_RX[i]);

    }

    printf("\n");

   }

   _task_block();

}

void read_task(uint32_t initial_data){

  MQX_FILE_PTR MaxSci1_dev = NULL;

  bool disable_rx = FALSE;

  rx_str.nCharRx = 0;

  MaxSci1_dev =  fopen( MaxSci1_CHANNEL, NULL );

  if (MaxSci1_dev == NULL) {printf("\nError opening Sci1");}

  else{printf("\nSci1 opned!");}

   while (TRUE) {

    fread(&(rx_str.data_buf_RX[rx_str.nCharRx]), 1, 1, MaxSci1_dev);

    if(rx_str.data_buf_RX[rx_str.nCharRx] == 0x0D){

    _lwsem_post(&lwsemUartRX);

    }

    rx_str.nCharRx++;

   }

}

You can see that the receive-task give the semaphore on the stop byte 0x0D, now I want that the semaphore will be give when elaps 200msec, so I need to implement a TimeOut that it will refresh every time I receive a char and when will be triggered it will give me the semaphpore.

There are two ways, I suppose, to do that

- Interrupt

-internal check on receive byte.

For the second choice one user of this community tell me this way:

Do

{

bytesRead = fread(inBuffer,1,1,fd);

                _time_get_elapsed_ticks(&lastByteTime);

                memcpy(&inPacket[inPacketSize], inBuffer, bytesReaded);

                inPacketSize += bytesReaded;

                _time_get_elapsed_ticks(&now);

} while (_time_diff_milliseconds(&now, &lastByteTime, &overflow) <250);

But do not work because last time the cycle do/while condition will be check on the first byte of another packet because on last byte check condition, that are ok and cycle another time, and stuck on fread until next packet.

So I’m asking, how to do a timeout on last byte with interrupt and how to with internal cycle (if possible) ? what is the best in efficiency?

Many thanks,

Massimiliano

4 Replies

2,658 Views
DavidS
NXP Employee
NXP Employee

Hi Massimiliano,

It has been long time since I created and tested my own custom read with a timeout.  I have attached that test file.  Hopefully it helps.

Regards,

David

2,658 Views
holyhope
Contributor III

Hi, many thanks for your answer.

I'm sorry for my delay but I have several problem.

today or next week I will test your routine and give you an answer.

sorry another time for delay and really many thanks for your help!

Massimiliano

@edit: sorry for delay, I can't test this routine now, I have study that and seems ok but I can't test now :-(

priority were reverse so this go in second stage... I will test as soon as possible and give you an answer!

Many thanks

0 Kudos
Reply

2,658 Views
tongjianwu
Contributor III

Hi  ,Massimiliano Sturla​

          How about your test ?

Thanks!

0 Kudos
Reply

2,658 Views
F50SC
Contributor III

Hi holyhope

How did you go with your problem with UART RX.

Were you able to receive and terminate after a timeout?

If so, could you share your solution?

Many thanks

0 Kudos
Reply