CW 10.6 Kinetis - "incompatible implicit declaration" of all math.h functions?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.6 Kinetis - "incompatible implicit declaration" of all math.h functions?

5,309 Views
dmarks_ls
Senior Contributor II

I've run into this previously on an earlier project, but it was easy to patch over because there was exactly one math reference.  This project is chock full of them, so I need to nip this in the bud.

 

Quite simply, it seems that #include <math.h> isn't doing any good, because the compiler isn't seeing any prototypes, and I'm getting a ton of messages like this:

 

../Sources/CalcLib/calcDenVisc.c: In function 'calcViscosity'

../Sources/CalcLib/calcDenVisc.c:81:9: warning: implicit declaration of function 'exp' [-Wimplicit-function-declaration]

../Sources/CalcLib/calcDenVisc.c: In function 'calcDensity':

../Sources/CalcLib/calcDenVisc.c:169:9: warning: implicit declaration of function 'pow' [-Wimplicit-function-declaration]

../Sources/CalcLib/calcDenVisc.c:176:9: warning: implicit declaration of function 'sqrt' [-Wimplicit-function-declaration]

../Sources/CalcLib/calcDenVisc.c:200:19: warning: incompatible implicit declaration of built-in function 'pow' [enabled by default]

../Sources/CalcLib/calcFlow.c: In function 'calcFlow':

../Sources/CalcLib/calcFlow.c:59:9: warning: implicit declaration of function 'fabs' [-Wimplicit-function-declaration]

../Sources/CalcLib/calcFlow.c:155:7: warning: incompatible implicit declaration of built-in function 'fabs' [enabled by default]

../Sources/CalcLib/calcFlow.c: In function 'updateHiResTot':

../Sources/CalcLib/calcFlow.c:233:7: warning: incompatible implicit declaration of built-in function 'fabs' [enabled by default]

../Sources/CalcLib/calcSupport.c: In function 'calcHdlr_doCalcStep':

../Sources/CalcLib/calcSupport.c:249:17: warning: implicit declaration of function 'sqrt' [-Wimplicit-function-declaration]

../Sources/CalcLib/calcSupport.c:258:17: warning: implicit declaration of function 'fabs' [-Wimplicit-function-declaration]

 

I'm running CW for MCU 10.6, with MQX v4.1.1 (had this issue with an MQX 4.0 project, too), compiling for a K20 120MHz target.  This is the only system library that I seem to have issues with.  Is there some special preprocessor define that I need to set in my project?  (I have _EWL_C99=1 and __VFPV4__=1 defined in the preprocessor.)

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

3,622 Views
trytohelp
NXP Employee
NXP Employee

David,

I've performed some tests on my side with a Hello project wizard example based on MCU v10.6 + MQX V4.1.1.

The math.h as other libraries are defined in the EWL lib.

By default the MQX project is using/including the EWL library but the options below is not selected..

            - this is the cause of the warning -

In fact if you include the #include <math.h>, the function fabs() for instance will not be resolved if the EWL is not enabled.

pastedImage_0.png

this option will add a command line instruction when the compiler is called: -specs=ewl_c_hosted.specs (in this configuration).

Now the math.h file will be really used to solve the math functions.

This is working for my example.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,623 Views
trytohelp
NXP Employee
NXP Employee

Hello David,

I will contact MQX colleague.

Keep you informed.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply