Hi All,
How to enable OTG2 to USB device mode in i.MX6 solo lite CPU ?
We had check with driver , OTG1 is OTG mode and OTG2 is fixed in USB Host mode.
We want to enable USB device only in OTG2
Does any patch can do it ?
Do you have the part number of the board you are using?
we are using the i.mx6 SABRESD board. You can find the detail info on www.freescale.com
Hi Qingrong,
Could you please using MX6SLEVK to test it ?
We are using i.MX6 solo lite CPU. (13mmx13mm package)
I have no MX6SLEVK board in my hand. I only have the MX6DQ board.
From the RM, it seems the OTG2 can't support device mode. Have you test the host mode for it?
dear sir.
does it mean OTG2 could support device mode or not ?
i can't understand the decription in linux reference manual.
It seems it can't support device mode due to the USB2PCI bridge connected.
dear Qingrong
thanks for your reply,
where is the USB to PCI bridge?,
it is connect to chip inside ?