imx6q mxc_sdc_fb timeout when waiting for flip irq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q mxc_sdc_fb timeout when waiting for flip irq

Jump to solution
37,487 Views
moseeneview
Contributor II

sometimes, my imx6q board gets timeout when waiting for flip irq    with rate 10~20%.

mxc_ipuv3_fb.c:

          it seems there's not irq to do complete. and then it wait_for_completion_timeout.

hwcomposer/hwc_vsync.cpp

          FBIO_WAITFORVSYNC error: time expire

i try as below, the issue also come out sometime. could u tell me why or some advice. thx.

1) Wait longer:    wait_for_completion_timeout(&mxc_fbi->flip_complete, 4*HZ);

2)  ldb_data = {

        .ipu_id = 1,          # or use ipu 0

        .disp_id = 0,

        .ext_ref = 1,

        .mode = LDB_SIN0,

  }

      or

ldb_data = {

        .ipu_id = 1,

        .disp_id = 0,

        .ext_ref = 1,

        .mode = LDB_SEP0,

        .sec_ipu_id = 1,

        .sec_disp_id =1,

}

3) fb_data = {

    { /*fb0*/

    .disp_dev = "ldb",

    .interface_pix_fmt = IPU_PIX_FMT_RGB666,

    .mode_str = "LDB-XGA",

    .default_bpp = 16,

    .int_clk = false,

    .late_init = true,             # or false

    },

}

4)

ipu_data[] = {

    {

    .rev = 4,

    .csi_clk[0] = "clko_clk",

    .bypass_reset = false,

    }, {

    .rev = 4,

    .csi_clk[0] = "clko_clk",

    .bypass_reset = false,

    },

};

1 Solution
24,228 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
29 Replies
8,483 Views
jameszt
Contributor II

Dear Freescale sir,

         Any update or solution for this issue?

         I met exactly the same issue on iMX6q board, light LVDS only.  plat_data->bypass_reset is false. 

        My kernel log has following lines,

                     imx6qvab820 user.info kernel: imx-ipuv3 2400000.ipu: IPU DMFC ONLY-DP HIGH RESOLUTION: 5B(0~3), 5F(4~7)
                      imx6qvab820 user.info kernel: imx-ipuv3 2800000.ipu: IPU DMFC ONLY-DP HIGH RESOLUTION: 5B(0~3), 5F(4~7)

        it will keep printing after system bootup, the LVDS is black.

                   user.err kernel: mxc_sdc_fb fb.24: timeout when waiting for flip irq

BRs

James        

0 Kudos
Reply
5,658 Views
ji_yun
Contributor II

Hi James ,

I met this same issue,you have solve this issue later? Have any advices?

 

Thanks,

0 Kudos
Reply
5,658 Views
LiuXuegang
NXP Employee
NXP Employee

I got one email from [email protected], the issue can't be reproduced if disable HWComposer by go to settings > developer options > check disable HW overlay.

Could you help further narrow down the issue follow below step?

1. Disable FSL hwcomposer by "mv /system/lib/hw/hwcomposer_fsl.imx6.so /system/lib/hw/hwcomposer_fsl.imx6.so.bak", the reboot board and test if the issue still happen or not.

2. If the issue still here after step 1, then disable Vivante hwcomposer by "mv /system/lib/hw/hwcomposer_viv.imx6.so /system/lib/hw/hwcomposer_viv.imx6.so.bak", reboot board and test if the issue still happen or not.

0 Kudos
Reply
5,658 Views
chrislin_wpi
Contributor II

Dear Sir,

We met the same question.
Do you have any idea for this issue?

Any point need to check?

0 Kudos
Reply
5,707 Views
pfsang
Contributor IV

hi, Mosee

     i had a try to change the frame rate(timing) and resolution.

    but haven't solved this issue .

Thanks,

peter

0 Kudos
Reply
5,707 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

From my point, some wrong IPU setting can cause the SYNC display error, then there will be "timeout when waiting for flip irq" error, but if you only modified the timing parameters for display mode, the test result should be same as original BSP.

0 Kudos
Reply
5,658 Views
tollerhecht
Contributor III

I am out of the office until 22.06.2014.

I will respond to your message when I return.

Note: This is an automated response to your message "Re:

- imx6q mxc_sdc_fb timeout when waiting for flip irq" sent on 06/20/2014

7:38:12 AM.

This is the only notification you will receive while this person is away.

0 Kudos
Reply
5,703 Views
pfsang
Contributor IV

hi, Qiang Li

    as you said, i decreased the frame rate, but it does not work.

    do you have the other method to fix it or what's root cause for the issue?

peter

0 Kudos
Reply
5,707 Views
mrleo
Contributor IV

Hi Mosee,

I met this same issue,.you have solve this issue later? Have any advices?

Thanks,

Leo

0 Kudos
Reply