LPDDR2 pin swapping on iMx6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR2 pin swapping on iMx6DL

1,947 Views
sebp20
Contributor I

Hi,

i am designing an board with a iMx6DL with 2 LPDDR2 (MT42L256M32D2) chips.

I noticed the LPDDR2 and DRAM pin mux mapping on page 3828 in the TRM.

Is bit swapping allowed on the data lines for easy pcb routing? Which are the restrictions?

Thanks

Sebastian

Labels (1)
0 Kudos
Reply
1 Reply

1,500 Views
Yuri
NXP Employee
NXP Employee

Strictly speaking, JEDEC provides pad sequence standardization for LPDDR2 :

Ordering of DQ bits shall be maintained in the system, including within the

package and on the PCB. DQ byte swapping and DQ bit Swapping are not allowed in

the system.

And MCIMX6SLEVK design follows such approach. In the same time i.MX53 design

with LPDDR2  does not : byte and bit within byte swapping is applied there.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply