Large inrush current at boot time on iMX6 SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Large inrush current at boot time on iMX6 SDB

2,277 Views
TMain
Contributor III

I have a question about the MCIMX6Q-SDB freescale dev kit board perhaps one of you can help me with.

I have noticed on boot and reset an average 3A current surge about 3 seconds into the boot process. This is on the auxiliary 5V supply and the duration of the peak is roughly 400uS.   I assume this has been encountered before. Do we know what causes this? Is it a peripheral or the processor itself?

Labels (1)
0 Kudos
Reply
2 Replies

1,996 Views
YixingKong
Senior Contributor IV

Todd, if Lin's answer helps you, please click Correct Answer.

Thanks,

Yixing

0 Kudos
Reply

1,996 Views
LinWang
NXP Employee
NXP Employee

Todd,

Please find below explantion:

"On the SD boards with the battery charger chips, current response through the battery charger ICs is not as responsive, so that larger in-rush currents will cause large voltage dips in the VIN supply to the PF0100 PMIC."

Lin

0 Kudos
Reply