mwldmcf.exe linker error for coldfire mcf52211(codewarrior v7.2)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mwldmcf.exe linker error for coldfire mcf52211(codewarrior v7.2)

2,763 Views
sureshandhe
Contributor I

I am getting the following linker error when i try to make a command line build(using makefile) for coldfire mcf52211 using codewarrior v7.2:

C:\\"Program Files"\Freescale\\"CodeWarrior for ColdFire V7.2"\ColdFire_Tools\Command_Line_Tools\mwldmcf.exe
-processor MCF521X -msgstyle gcc -lavender model="ewl",print="int",scan="int",io="buffered" -main "__startup"
-force_active '__vect','__cfm' -sreclength 32 -breclength 252 -sreceol unix -keeplocal off -nodeadstrip -listing
-show all -warn on -g  lcf\MCF52211_INTERNAL_FLASH.lcf
... list of object files ...
-o bin\MCF52211_INTERNAL_FLASH.elf
mwldmcf.exe: warning: Specified file 'v2\libm.a' not found
mwldmcf.exe: warning: Specified file 'v2\libc.a' not found
mwldmcf.exe: warning: Specified file 'v2\librt.a' not found
mwldmcf.exe: warning: Specified file 'fp_coldfire.a' not found
mwldmcf.exe: unable to find EWL lib:
mwldmcf.exe: v2\libm.a

I set the following environment variables but for some reason linker is not able to find the library path:

CWFolder       :  'C:\Program Files\Freescale\CodeWarrior\CodeWarrior for ColdFire V7.2'
CWINSTALL      :  'C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2'
LM_LICENSE_FILE:  %CWFolder%\license.dat
MWCIncludes    :  %CWFolder%\ColdFire_Support\ewl\EWL_C\Include; %CWFolder%\ColdFire_Support\ewl\EWL_C\Include\sys
MWLibraries    :  %CWFolder%\ColdFire_Support\ewl\lib

Any help to resolve this issue?

Labels (1)
0 Kudos
Reply
2 Replies

2,329 Views
sureshandhe
Contributor I

I tried following two sets of environment variables but nothing worked(not sure which one mwldmcf likes):

Set1:
-----
CWFolder:
'C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2'

CWINSTALL:
'C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2'

LM_LICENSE_FILE:
'C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\license.dat'

MWCIncludes:
'C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\ColdFire_Support\ewl\EWL_C\include'; 'C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\ColdFire_Support\ewl\EWL_C\include\sys'

MWLibraries:
'C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\ColdFire_Support\ewl\lib'

Set2:
-----
CWFolder:
C:\\"Program Files"\Freescale\\"CodeWarrior for ColdFire V7.2"

CWINSTALL:
C:\\"Program Files"\Freescale\\"CodeWarrior for ColdFire V7.2"

LM_LICENSE_FILE:
C:\\"Program Files"\Freescale\\"CodeWarrior for ColdFire V7.2"\license.dat

MWCIncludes:
C:\\"Program Files"\Freescale\\"CodeWarrior for ColdFire V7.2"\ColdFire_Support\ewl\EWL_C\include'; C:\\"Program Files"\Freescale\\"CodeWarrior for ColdFire V7.2"\ColdFire_Support\ewl\EWL_C\include\sys

MWLibraries:
C:\\"Program Files"\Freescale\\"CodeWarrior for ColdFire V7.2"\ColdFire_Support\ewl\lib

Please help me to resolve this issue.

0 Kudos
Reply

2,329 Views
CrasyCat
Specialist III

Hello

Did you try setting MWLibraries to

  "C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\ColdFire_Support\ewl\lib\v2"; "C:\Program Files\Freescale\CodeWarrior for ColdFire V7.2\ColdFire_Support\ewl\lib"

and set MWLibraryFiles to libc.a;librt.a;libm.a;fp_coldfire.a

Additionally for some reason you have some times two backslashes and sometimes just one in the path specification. Not sure how this one is build up, and why this is so...

CrasyCat

0 Kudos
Reply