otg device mode issue for imx535 QSB ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

otg device mode issue for imx535 QSB ?

Jump to solution
2,634 Views
venkateshp
Contributor I

Hi,

    I was used IMx53 development kit and USB OTG DEVICE issue is their.How to configure OTG in device mode  and let me know the OTG Id pin is connected to External  5V or Ground,otherwise Otg id pin connecd to Both Ext 5V or Ground which one is DEVICE MOD.

thanks,

Venkat

Labels (3)
0 Kudos
Reply
1 Solution
1,845 Views
Henry_p
NXP Employee
NXP Employee

You don't need to connect ID pin to 5V or ground for device function. Just keep it floating.

You can find more details in USB On-The-Go - Wikipedia, the free encyclopedia

View solution in original post

0 Kudos
Reply
2 Replies
1,845 Views
venkatesh_pvsm
Contributor II

Hi ,

  Still Devcice mode was not detected in i.MX53 QSB Board, How to solve this issue.

Thanks By,

Venkat.

0 Kudos
Reply
1,846 Views
Henry_p
NXP Employee
NXP Employee

You don't need to connect ID pin to 5V or ground for device function. Just keep it floating.

You can find more details in USB On-The-Go - Wikipedia, the free encyclopedia

0 Kudos
Reply