K60 for time triggered Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 for time triggered Ethernet

Jump to solution
2,357 Views
tenfy
Contributor I

      I want to ask some question about Kneits

      As we know,K60 micro process is supporting  the agreement of 1588,it also means that it can make synchronization  come true.so i want to achieve time triggered Ethernet based on the 1588 clock synchronization .

      I just want to ask whether this plan can be achieved.Another question is that has freescale done the Development Boards achieving time triggered Ethernet based on the 1588 clock synchronization .

                                                                                                     Best Regards

                                                                                                        Yours:Tenfy

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,926 Views
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Tenfy,

Freescale is working with the IXXAT partner to deliver a stack that work under the Kinetis microcontrollers using MQX and the IXXAT IEEE 1588 V2 stack. The development is in progress and unfortunately we don’t have a target date for this release. You could contact directly with IXXAT (http://www.ixxat.com/ ) asking for any solution that could be used at this time.

Have a nice day!

-Garabo

View solution in original post

0 Kudos
Reply
1 Reply
1,927 Views
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Tenfy,

Freescale is working with the IXXAT partner to deliver a stack that work under the Kinetis microcontrollers using MQX and the IXXAT IEEE 1588 V2 stack. The development is in progress and unfortunately we don’t have a target date for this release. You could contact directly with IXXAT (http://www.ixxat.com/ ) asking for any solution that could be used at this time.

Have a nice day!

-Garabo

0 Kudos
Reply