K60 Ethernet 1588 Capabilities when used with non 1588 PHY's

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 Ethernet 1588 Capabilities when used with non 1588 PHY's

Jump to solution
2,698 Views
pmt
Contributor V

 

The K60 series comes with Ethernet 1588 capabilities.  My question is does the 1588 provide any useful incremental functionality when not using the 1588 hardware clocking lines, or using a non-1588 capable PHY?  That is, is the 1588 hardware internal to the K60 able to operate at the Ethernet packet level and provide some level of time synchronization benefit, or is external hardware a requirement to make this useful?

 

  

0 Kudos
Reply
1 Solution
2,216 Views
pmt
Contributor V

I found a nice application note from Freescale that answers my own question.  Sub-microsecond resolution is possible without a 1588 PHY. 

View solution in original post

0 Kudos
Reply
2 Replies
2,216 Views
tenfy
Contributor I

The K60 have a internal MAC which support 1588 clock,so we just need a common PHY to come true the 1588 clock synchronization.

0 Kudos
Reply
2,217 Views
pmt
Contributor V

I found a nice application note from Freescale that answers my own question.  Sub-microsecond resolution is possible without a 1588 PHY. 

0 Kudos
Reply