USB OC signal level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB OC signal level

3,767件の閲覧回数
juergene
Contributor III

Hello Yuri,

unfortunately, it is not clear what kind of logic level the OC-pin (overcurrent) has.

In our design we have a power switch which indicates the OC-signal as low active. But if we implement the OC-signal in our software it will always detect overcurrent an shutdown the powerswitch.

Is the OC-signal now low or high active ?

Thanks in advance!

Best regards,

Juergen

#i.mx8m‌

0 件の賞賛
返信
1 返信

3,638件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   It is assumed, that active level of the USB OC signal is LOW.

For i.MX8M GPIO LOW level specs should be taken in consideration.

Use table "GPIO DC parameters", parameter "Low-level input voltage"

in i.MX8M Datasheets (Hardware Specs).  

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信