A: Download: Desktop and Hardware Demos
Request for Window Builder - The free download is the full version of Window Builder, but no source code is provided, so applications can only be developed on provided compiled libraries (this by default is Windows, but can be extended to a EVB such as the Tower System).
Request for further evaluation please contact Freescale sales or distributor representative.
A: Yes, PEG Software can be licensed for for NON-Freescale and Freescale silicon. There is a discount when used with Freescale silicon.
A: There are 4 licensing models.
1) PEG Base Single Product/MCU (3 seats, <=10,000 units, 1 year support) is specific to the processor used AND the specific name and model of the customer end product.
2) Upgrade - Unlimited Run-time for PEG Base: There are NO limits on the number of run-time units for the PEG Base Single Product/MCU
3) Upgrade - Same MCU across Product Family (+3 seats, unlimited run-time): Supports a family of customer end products that use the same processor
4) Upgrade - Multi MCU across Product Family (+6 seats, unlimited run-time): Supports a family of customer end products that use multiple processors
A: One year of support is included with the purchase of a license and can always renew.
A: PEG implemented a scheduler that runs at a defined rate (20 times per second by default) and quickly checks a messaging queue. If updates to the image are required, then the appropriate actions are taken to update the screen.
A: PEG will define the require space for the frame buffer depending on the screen resolution, color depth, and number of buffers (i.e double-buffering, multiple surfaces, etc…)
A: There are examples of PEG drawing a variety of graphs (in the demo folder of PEG).
A: PEG screen drivers can be developed for virtually any processor/controller. The list here includes devices for which drivers currently exist.
A: You can purchase it direct please contact [email protected] or from a number of distributors/re-sellers:
- eCOS
- eSOL
- Quadros
- Arrow
- Future
- Advent