Zumo Robot with FRDM-KW41

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zumo Robot with FRDM-KW41

Zumo Robot with FRDM-KW41

Description

In this demo we show how to create a zumo robot basic controller. For this we will use the FRDM-KW41 card, an H bridge, and a cell phone with the NXP IoT toolbox application. From the application we will send the characters F forward, S to stop, B to back, L to left, R to right.

The FRDM-KW41Z highly-sensitive, optimized 2.4 GHz radio features a PCB F-antenna which can be bypassed to test via SMA connection, multiple power supply options, push/capacitive touch buttons, switches, LEDs and integrated sensors.

Video

(view in My Videos)

Diagram and Schematic

zumo block diagram.png

Zumo demo schematic.png

Step by Step guide

  1. First, we need to have MCUXpresso installed and open.
  2. Download and load the Zumo Robot project in MCUXpresso.
  3. Install NXP IoT Toolbox app.
  4. Compile the project, connect the board and load it.
  5. Connect the card as indicated in the schematic
  6. Connect the power supply.
  7. Press switch 4 on the board.
  8. Open NXP IoT Toolbox, select Wireles UART and connect with the board.
  9. Now you can send the characters mentioned in the description.

NXP ProductLink
Freedom Development Kit for Kinetis® KW41Z/31Z/21Z MCUsFRDM-KW41Z |Bluetooth Thread Zigbee enabled Freedom Development Kit | NXP 
Labels (1)
Attachments
No ratings
Version history
Last update:
‎10-14-2019 06:38 AM
Updated by: